:MEASure:MTESt:MUNCertainty:LOCation?
Query Syntax
:MEASure:MTESt{N}:MUNCertainty:LOCation?
{N} identifies a specific mask and must be a value from 1 to 16. For example, :MTESt2 selects mask 2.
Description
Returns an index for the location of the MUNCertainty measurement results in the active measurement list. Using this information, you can select, clear, or remove measurement results from the displayed results table. If the measurement is not listed in the table, a "−1" is returned.