:MEASure:MTESt:NWAVeforms?
Query Syntax
:MEASure:MTESt{N}:NWAVeforms?
{N} identifies a specific mask and must be a value from 1 to 16. For example, :MTESt2 selects mask 2.
Description
Returns the number of Waveforms reported in the Masks Tests results table during eye mask testing. This is the total number of waveforms acquired since the mask test was started.