:MEASure:MTESt:THITs:STATus:REASon?

Query Syntax

:MEASure:MTESt{N}:THITs:STATus:REASon?

{N} identifies a specific mask and must be a value from 1 to 16. For example, :MTESt2 selects mask 2.

Query Response

Refer to the table "Common Reasons for INV or QUES Status".

Description

Returns a string that explains the reason for a failed :MEASure:MTESt:THITs? measurement. If the measurement was successful, a null string is returned.

Additional information about the failure may be available using the :MEASure:MTESt:THITs:STATus:DETails? sibling query. Use the :MEASure:MTESt:THITs:STATus? parent query to determine if the measurement has failed.

See Also