:MEASure:MTESt:TWAVeforms?
Query Syntax
:MEASure:MTESt{N}:TWAVeforms?
{N} identifies a specific mask and must be a value from 1 to 16. For example, :MTESt2 selects mask 2.
Description
Returns the number of Tested Waveforms reported in the Masks Tests results table during eye mask testing. Tested Waveforms may or may not be equal to the total number of waveforms. If mask test was turned on initially and there have been no mask scale changes, then Tested Waveforms will equal number of Total Waveforms. However, mask scale changes can make the Tested Waveforms less than Total Waveforms. Tested Waveforms can be questionable when the mask scale changes because the past number of Tested Waveforms is deleted, and only the last waveform is tested.