:MEASure:MTESt:UINTervals:STATus:DETails?
Query Syntax
:MEASure:MTEStN:UINTervals:STATus:DETails?
Description
Returns a string that may provide additional details for a failed :MEASure:MTESt:UINTervals? measurement. If the measurement was successful, a null string is returned.
For a basic description of a measurement failure, use the :MEASure:MTESt:UINTervals:STATus:REASon? sibling query. Use the :MEASure:MTESt:UINTervals:STATus? parent query to determine if the measurement has failed.