:MEASure:PAM:RFTime:TRANsition

Command Syntax

:MEASure:PAM:RFTime:TRANsition {TRANsition01 | TRANsition02 | TRANsition03 
   | TRANsition12 | TRANsition13 | TRANsition23}

Query Syntax

:MEASure:PAM:RFTime:TRANsition?

Description

Selects the level-to-level transition of a PAM signal that will be measured when the :MEASure:PAM:RFTime parent command is sent. PAM4 signals have six possible level-to-level transitions: 0-1, 0-2, 0-3, 1-2, 1-3, and 2-3. PAM3 signals have three possible level-to-level transitions: 0-1, 0-2, and 1-2.

Whether the edge is rising or falling is specified by the :MEASure:PAM:RFTime:EDIRection command.