:MEASure:PAM:RMS:LEVel
Command Syntax
:MEASure:PAM:RMS:LEVel {LEVel0 | LEVel1 | LEVel2 | LEVel3}
Query Syntax
:MEASure:PAM:RMS:LEVel?
Description
Selects the level of a PAM or NRZ signal that will be measured when the :MEASure:PAM:RMS parent command is sent. PAM4 signals have four possible levels: 0, 1, 2, and 3. PAM3 signals have three possible levels: 0, 1, and 2. NRZ signals has two possible levels: 0 and 1.
| Arguments | Description | |
|---|---|---|
| LEVel3 | Selects level 3. |
|
| LEVel2 | Selects level 2. | |
| LEVel1 | Selects level 1. | |
| LEVel0 | Selects level 0. | |
Example Command Sequence
:MEASure:PAM:RMS:LEVel LEVel2