:MEASure:PJITter:DDIRac:TUDJ?
Query Syntax
:MEASure:PJITterN:DDIRac:TUDJ?
Where N identifies one of four possible PAM jitter analyses {1:4}. For example, PJITter4.
Description
For the selected row in the Dual-Dirac PAM Jitter measurements table (see :MEASure:PJITter:DDIRac:SELect), this query returns the Uncorrelated Deterministic Jitter Delta-Delta (TTX-UDJDD) measurement from that row.