:MEASure:PJITter:DDIRac:SELect

Command Syntax

:MEASure:PJITterN:DDIRac:SELect <table_row_number>
            

Where N identifies one of four possible PAM jitter analyses {1:4}. For example, PJITter4.

<table_row_number> is an integer.

Query Syntax

:MEASure:PJITterN:DDIRac:SELect?

Description

This command selects a row number in Dual-Dirac PAM Jitter measurements table.

With the PCIe Dual-Dirac 52-symbol pattern, the 12 edges possible in PAM4 each occur four times, and the first row contains the averaged measurements, so there will be 49 rows in the table.

Use the :MEASure:PJITter:DDIRac:EDGE? query to get the edge number associated with the selected table row.

Use the :MEASure:PJITter:DDIRac:TRANsition? query to get the "Level to Level" transition associated with the selected table row.