:MEASure:SNDRatio:SERRor
Command Syntax
:MEASure:SNDRatio:SERRor
Query Syntax
:MEASure:SNDRatio:SERRor?
Description
This is an AC Vrms (standard deviation) measurement on the linear fit error e(k) waveform.
The linear fit error is the difference between the actual transmitter output signal and the linear fit Pulse Corrected waveform. It represents essentially the distortion from a linear response.
SNDR measurement parameters are defined for the waveform source selected by :MEASure:SNDRatio:SERRor:SOURce.
Example Command Sequence
:MEASure:SNDRatio:SERRor:SOURce CHANnel1 :CHANnel1:SNDRatio:STANdard PCIe :CHANnel1:SNDRatio:PUINterval 32 :CHANnel1:SNDRatio:NAVerages 8 :CHANnel1:SNDRatio:LFPLength 600 :CHANnel1:SNDRatio:LFPDelay 8 :MEASure:SNDRatio:SERRor :MEASure:SNDRatio:SERRor?