:MEASure:SNDRatio:SERRor:STATus:DETails?
Query Syntax
:MEASure:SNDRatio:SERRor:STATus:DETails?
Description
Returns a string that may provide additional details for a failed :MEASure:SNDRatio:SERRor measurement. If the measurement was successful, a null string is returned.
For a basic description of a measurement failure, use the :MEASure:SNDRatio:SERRor:STATus:REASon? sibling query. Use the :MEASure:SNDRatio:SERRor:STATus? parent query to determine if the measurement has failed.