:MEASure:VERTical:OVERshoot:EDIRection
Command Syntax
:MEASure:VERTical:OVERshoot:EDIRection {RISing | FALLing}
Query Syntax
:MEASure:VERTical:OVERshoot:EDIRection?
Description
For the :MEASure:VERTical:OVERshoot measurement, this command specifies which signal edges to include in the measurement.
Example Command Sequence
:MEASure:VERTical:OVERshoot:SOURce CHAN1_1 :MEASure:VERTical:OVERshoot:EDIRection RISing :MEASure:VERTical:OVERshoot :MEASure:VERTical:OVERshoot?