:MEASure:VERTical:OVERshoot:OCCurrences

Command Syntax

:MEASure:VERTical:OVERshoot:OCCurrences  {ONE | ALL}

Query Syntax

:MEASure:VERTical:OVERshoot:OCCurrences?

Description

This command lets you select between Measure One and Measure All in the user interface which specifies whether Infiniium should make one edge-related measurement per acquisition or multiple measurements per acquisition using all edges in the acquisition.

When Measure One is selected:

  • Measurements using edges are made on a particular edge (or pair of edges). Measurements are made on the edge closest to the timebase reference (see :TIMebase:REFerence).
  • Measurement statistics are calculated for the one specific edge only and compiled over a number of acquisitions. A Single acquisition adds a single value to the measurement statistics. All other edges are ignored.

When Measure All is selected:

  • Measurements using edges are made on all edges (or all pairs of edges) in the acquisition.
  • The "Current" measurement result (see :MEASure:RESults?) is taken from the measurement closest to the timebase reference. For measurements on memory waveforms, it is the measurement closest to the horizontal X position setting. Annotations are shown at the "Current" measurement result.

Switching between Measure One and Measure All restarts the measurement count.

Query Response

{ONE | ALL}