:MEASure:VERTical:PPHRatio:STATus?

Query Syntax

:MEASure:VERTical:PPHRatio:STATus?

Query Response

{CORR | INV | QUES}
CORR
The measurement result is correct.
INV
The measurement result is invalid. A question mark (?) is shown in the displayed results table instead of a measurement result.
QUES
The measurement result is questionable. A question mark (?) is shown in the displayed results table next to the measurement result.

Description

Queries the status of the Peak-Peak at Hit Ratio measurement (:MEASure:VERTical:PPHRatio). Use the :MEASure:VERTical:PPHRatio:STATus:REASon? child query to determine the reason for an invalid or questionable measurement. Additional information about the failure may be available using the :MEASure:VERTical:PPHRatio:STATus:DETails? child query.

See Also

Measurement Identification

Avoid subtle programming errors! To ensure that the correct measurement is installed or queried, always explicitly identify a measurement when installing a measurement or querying a measured value, status, or detail. To identify a measurement, specify the measurement's source waveform (:SOURce child command). With some measurements, you may also need to specify other identifying values. Generally, when selecting a measurement using Infiniium's GUI, if a dialog appears prompting you to select values, you should explicitly specify these values when remotely identifying the measurement.

For example, to return the status of the :MEASure:VERTical:PPHRatio measurement:

Infiniium.write(':MEASure:VERTical:PPHRatio:SOURce CHAN1_1')
if Infiniium.query(':MEASure:VERTical:PPHRatio:STATus?') == 'CORR';
    measurement = Infiniium.query(':MEASure:VERTical:PPHRatio?')