:MEASure:VERTical:PPHRatio:THRatio

Command Syntax

:MEASure:VERTical:PPHRatio:THRatio <hit_ratio>

<hit_ratio> is a double from 0.0 to 0.1.

Query Syntax

:MEASure:VERTical:PPHRatio:THRatio?

Description

Sets the hit ratio value for the Peak-Peak at Hit Ratio measurement (:MEASure:VERTical:PPHRatio). The default hit ratio is 1.0E-2 which is called out in the IEEE 802.3cu standard. The minimum value is 0.0. The maximum value is 0.1.