:MEASure:VERTical:PREShoot:EDIRection
Command Syntax
:MEASure:VERTical:PREShoot:EDIRection {RISing | FALLing}
Query Syntax
:MEASure:VERTical:PREShoot:EDIRection?
Description
For the :MEASure:VERTical:PREShoot measurement, this command specifies which signal edges to include in the measurement.
Example Command Sequence
:MEASure:VERTical:PREShoot:SOURce CHAN1_1 :MEASure:VERTical:PREShoot:EDIRection RISing :MEASure:VERTical:PREShoot :MEASure:VERTical:PREShoot?