:MEASure:VERTical:PREShoot:FAVorite

Command Syntax

:MEASure:VERTical:PREShoot:FAVorite {ON | OFF | 1 | 0}

Query Syntax

:MEASure:VERTical:PREShoot:FAVorite?

Query Response

{1 | 0}

Description

Adds this measurement to, or removes it from, the Favorites category in the graphical user interface's Add Measurements dialog box.