:MEASure:VERTical:VAVerage:EDIRection
Command Syntax
:MEASure:VERTical:VAVerage:EDIRection {RISing | FALLing}
Query Syntax
:MEASure:VERTical:VAVerage:EDIRection?
Description
For the Average amplitude measurement, when the selected area is a single cycle:
RISingorFALLing— the cycle beginning with this edge that is nearest to the timebase reference is the cycle to measure.