:MEASure:VERTical:VAVerage:UREFerence:VALue

Command Syntax

:MEASure:VERTical:VAVerage:UREFerence:VALue <time_location>

<time_location> is a double.

Query Syntax

:MEASure:VERTical:VAVerage:UREFerence:VALue?

Description

When a user-defined horizontal reference location is enabled (see :MEASure:VERTical:VAVerage:UREFerence:STATe), this command specifies its time location with respect to the trigger (t = 0) location.