:REGions:REGion{N}:STATe

Command Syntax

:REGions:REGion{1:8}:STATe {ON | OFF | 1 | 0}

Query Syntax

:REGions:REGion{1:8}:STATe?

Query Response

{1 | 0}

Description

Enables or disables the specified region.

Regions let you restrict the data used for a measurement to a specific area of the source waveform as defined by left and right X-axis limits.

Use the :REGions:REGion{N}:X{1:2} command to set the x-axis boundaries for each region.

After defining one or more regions, use the :REGion child command of a specific measurement to apply a region to the measurement. For example, limit a rise-time measurement to the data within region 3, use the following command:

:MEASure:HORizontal:RTIMe:REGion REGion3

The Jitterp-p and Jitterrms measurements cannot be made on a region.

Example Command Sequence

:REGions:REGion1:X1 40E-12
:REGions:REGion1:X2 100E-12
:REGions:REGion1:STATe ON
:MEASure:HORizontal:RTIMe:SOURce CHAN1_1
:MEASure:HORizontal:RTIMe:REGion REGion1
:MEASure:HORizontal:RTIMe
:MEASure:HORizontal:RTIMe?