:REGions:REGion{N}:SOURce
Command Syntax
:REGions:REGion{1:8}:SOURce {CHANnel{N} | DIFF{1:8}{A|C} | FUNCtion{1:64} | WMEMory{1:8}}
{N} identifies a specific channel in the form "<connection1-8>_<ch1-8>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1-8>". For example, connection 4 channel 2 is CHANnel4_2.
Query Syntax
:REGions:REGion{1:8}:SOURce?
Description
This command specifies the waveform source the region applies to.
Regions let you restrict the data used for a measurement to a specific area of the source waveform as defined by left and right X-axis limits.
Use the :REGions:REGion{N}:X{1:2} command to set the x-axis boundaries for each region.
After defining one or more regions, use the :REGion child command of a specific measurement to apply a region to the measurement. For example, limit a rise-time measurement to the data within region 3, use the following command:
:MEASure:HORizontal:RTIMe:REGion REGion3
The Jitterp-p and Jitterrms measurements cannot be made on a region.
Example Command Sequence
:REGions:REGion1:SOURce CHAN1_1 :REGions:REGion1:X1 40E-12 :REGions:REGion1:X2 100E-12 :REGions:REGion1:STATe ON :MEASure:HORizontal:RTIMe:SOURce CHAN1_1 :MEASure:HORizontal:RTIMe:REGion REGion1 :MEASure:HORizontal:RTIMe :MEASure:HORizontal:RTIMe?