:SYSTem:SOFTware:LICenses:BORRow?
Query Syntax
:SYSTem:SOFTware:LICenses:BORRow? <license_model_number><number_of_days>
Where <_model_number_license> specifies the package license using the string listed in the following Software License Package Arguments table.
Where <number_of_days> is an integer that specifies how many days you wish to borrow the license. The valid range of days is 1 to 90.
Query Response
Boolean, 1 or 0
Description
Use this query to borrow a software license package from Keysight's Software Manager Utility. You must specify both the package license and the number of days that you wish to use (borrow) the license. The query returns a '1' if the license was successfully borrowed and a '0' if the borrow failed.
Example
:SYSTem:SOFTware:LICenses:BORRow? "D9320JITA" 90