:SYSTem:SOFTware:LICenses:FEATure?

Query Syntax

:SYSTem:SOFTware:LICenses:FEATure? "<license_model_number>"

Where <license_model_number> is the model number string representing a license.

Query Response

String identifying feature. For example, "D9320JITA".

Description

If the parameter identifies a licensed feature, for example "D9320JITA" the model number string for the package is returned. For example, "D9320JITA".

Be sure to enclose the parameter with quote characters. Entering an other parameter (or no parameter) results in an –224, Illegal parameter value message.

Example Query

:SYSTem:SOFTware:LICenses:FEATure? "D9320JITA"