:TIMebase:INTerpolate:FACTor

Command Syntax

:TIMebase:INTerpolate:FACTor <number_interpolation_points>

<number_interpolation_points> is an integer.

Query Syntax

:TIMebase:INTerpolate:FACTor?

Description

When automatic interpolation is off (see :TIMebase:INTerpolate:AUTO) and Sin(x)/x interpolation is selected (see :TIMebase:INTerpolate:METHod), this command specifies an integer value of 2, 4, 8, 16, or 32 interpolated points between the actually sampled points.