:TIMebase:INTerpolate:METHod
Command Syntax
:TIMebase:INTerpolate:METHod {NONE| SINC}
Query Syntax
:TIMebase:INTerpolate:METHod?
Description
When automatic interpolation is off (see :TIMebase:INTerpolate:AUTO), this command provides these options:
- SINC
- Selects sin(x)/x interpolation with the number of interpolated points between actual samples specified by the
:TIMebase:INTerpolate:FACTorcommand. - NONE
- Turns interpolation off altogether.