:TRIGger:EDGE:COUPling
Command Syntax
:TRIGger:EDGE:COUPling {DC}
Query Syntax
:TRIGger:EDGE:COUPling?
Description
In the Edge trigger mode (see :TRIGger:MODE), this command specifies the coupling for the trigger source:
-
DC— Allows DC and AC signals into the trigger path.
Note that edge trigger coupling is independent of channel coupling.