:TRIGger:MODE
Command Syntax
:TRIGger:MODE {HBEDge | EDGE | GLITch | PWIDth | PATTern | RUNT | SHOLd | TRANsition | DELay | TIMeout | WINDow}
Query Syntax
:TRIGger:MODE?
Description
This command selects the trigger mode:
HBEDge— High Bandwidth Edge. See :TRIGger High Bandwidth Edge Commands.EDGE— Edge. See :TRIGger Edge Commands.GLITch— Glitch. See :TRIGger Glitch Commands.PWIDth— Pulse Width. See :TRIGger Pulse Width Commands.PATTern— Pattern. See :TRIGger Pattern Commands.RUNT— Runt. See :TRIGger Runt Commands.SHOLd— Setup And Hold. See :TRIGger Setup And Hold Commands.TRANsition— Edge Transition. See :TRIGger Edge Transition Commands.DELay— Edge Then Edge. See :TRIGger Edge Then Edge Commands.TIMeout— Timeout. See :TRIGger Timeout Commands.WINDow— Window. See :TRIGger Window Commands.