:TRIGger:PWIDth:MODE
Command Syntax
:TRIGger:PWIDth:MODE {LTHan | GTPend | GTTimeout | RINSide | ROUTside}
Query Syntax
:TRIGger:PWIDth:MODE?
Description
In the Pulse Width trigger mode (see :TRIGger:MODE), this command selects what kind of pulses will cause a trigger:
LTHan— Pulses narrower than the specified:TRIGger:PWIDth:WIDTh. This is the same as the Glitch mode (see :TRIGger Glitch Commands).GTPend— Pulses wider than the specified:TRIGger:PWIDth:WIDTh, triggering when the pulse ends.GTTimeout— Pulses wider than the specified:TRIGger:PWIDth:WIDTh, triggering when the width is exceeded. This is the same as the Timeout mode (see :TRIGger Timeout Commands).RINSide— Pulses within the range specified by the:TRIGger:PWIDth:RSTartand:TRIGger:PWIDth:RENDvalues.ROUTside— Pulses outside the range specified by the:TRIGger:PWIDth:RSTartand:TRIGger:PWIDth:RENDvalues.