:TRIGger:SEQuence:PWIDth:REND

Command Syntax

:TRIGger:SEQuence{A|B}:PWIDth:REND <seconds>

<seconds> is a double.

Query Syntax

:TRIGger:SEQuence{A|B}:PWIDth:REND?

Description

In the Pulse Width trigger mode (see :TRIGger:SEQuence:MODE), when triggering when the pulse width is inside or outside a range (see :TRIGger:SEQuence:PWIDth:MODE), this command specifies the upper range of the width.