:TRIGger:SEQuence:PWIDth:WIDTh

Command Syntax

:TRIGger:SEQuence{A|B}:PWIDth:WIDTh <seconds>

<seconds> is a double.

Query Syntax

:TRIGger:SEQuence{A|B}:PWIDth:WIDTh?

Description

In the Pulse Width trigger mode (see :TRIGger:SEQuence:MODE), when triggering when the pulse width is less than or greater than a specified time (see :TRIGger:SEQuence:PWIDth:MODE), this command specifies the amount of time.