:TRIGger:SEQuence:WINDow:MODE

Command Syntax

:TRIGger:SEQuence{A|B}:WINDow:MODE  {ENTering | EXITing | IVRCross | IVRTimeout | IVRLess | OVRCross | OVRTimeout | OVRLess}

Query Syntax

:TRIGger:SEQuence{A|B}:WINDow:MODE?

Description

In the Window trigger mode (see :TRIGger:SEQuence:MODE), this command selects the window condition to trigger on:

  • ENTering — Triggers when the signal enters the voltage range.
  • EXITing — Triggers when the signal exits the voltage range.
  • IVRCross — When the signal is inside the voltage range for greater than the specified :TRIGger:SEQuence:WINDow:TIME, the trigger occurs when the signal crosses one of the voltage range boundaries.
  • IVRTimeout — When the signal is inside the voltage range for greater than the specified :TRIGger:SEQuence:WINDow:TIME, the trigger occurs when the time is exceeded.
  • IVRLess — Triggers when the signal is inside the voltage range for less than the specified :TRIGger:SEQuence:WINDow:TIME.
  • OVRCross — When the signal is outside the voltage range for greater than the specified :TRIGger:SEQuence:WINDow:TIME, the trigger occurs when the signal crosses one of the voltage range boundaries.
  • OVRTimeout — When the signal is outside the voltage range for greater than the specified :TRIGger:SEQuence:WINDow:TIME, the trigger occurs when the time is exceeded.
  • OVRLess — Triggers when the signal is outside the voltage range for less than the specified :TRIGger:SEQuence:WINDow:TIME.