:TRIGger:SEQuence:WINDow:TIME
Command Syntax
:TRIGger:SEQuence{A|B}:WINDow:TIME <seconds>
<seconds> is a double.
Query Syntax
:TRIGger:SEQuence{A|B}:WINDow:TIME?
Description
In the Window trigger mode (see :TRIGger:SEQuence:MODE), when triggering on a condition that is greater or less than an amount of time (see :TRIGger:SEQuence:WINDow:MODE), this command specifies the amount of time.