:TRIGger:TRANsition:TIME
Command Syntax
:TRIGger:TRANsition:TIME <seconds>
<seconds> is a double.
Query Syntax
:TRIGger:TRANsition:TIME?
Description
In the Edge Transition trigger mode (see :TRIGger:MODE), when triggering on a transition that is longer or shorter than specified time (see :TRIGger:TRANsition:MODE), this command specifies the amount of time.