:TRIGger:WINDow:MODE
Command Syntax
:TRIGger:WINDow:MODE {ENTering | EXITing | IVRCross | IVRTimeout | IVRLess | OVRCross | OVRTimeout | OVRLess}
Query Syntax
:TRIGger:WINDow:MODE?
Description
In the Window trigger mode (see :TRIGger:MODE), this command selects the window condition to trigger on:
ENTering— Triggers when the signal enters the voltage range.EXITing— Triggers when the signal exits the voltage range.IVRCross— When the signal is inside the voltage range for greater than the specified:TRIGger:WINDow:TIME, the trigger occurs when the signal crosses one of the voltage range boundaries.IVRTimeout— When the signal is inside the voltage range for greater than the specified:TRIGger:WINDow:TIME, the trigger occurs when the time is exceeded.IVRLess— Triggers when the signal is inside the voltage range for less than the specified:TRIGger:WINDow:TIME.OVRCross— When the signal is outside the voltage range for greater than the specified:TRIGger:WINDow:TIME, the trigger occurs when the signal crosses one of the voltage range boundaries.OVRTimeout— When the signal is outside the voltage range for greater than the specified:TRIGger:WINDow:TIME, the trigger occurs when the time is exceeded.OVRLess— Triggers when the signal is outside the voltage range for less than the specified:TRIGger:WINDow:TIME.