Electrical Connector Care

Damage to electrical input connectors (as well as connectors on calibration and verification devices, test ports, cables, and other devices) can degrade measurement accuracy and damage instruments. Replacing a damaged electrical connectors can cost thousands of dollars, not to mention lost time! This expense can be avoided by observing the important precautions described in the topics referenced below.

To avoid expensive damage while making the final connection, select one of the following procedures for proper torque wrench and handling techniques. This guarantees a perfectly tight, consistent connections while preventing connector damage:

The drawings in this topic illustrate the proper handling of a torque wrench when making 1mm and 2.4 mm input connection. The general techniques can be applied to other connectors as well.

The input circuits can be damaged by electrostatic discharge (ESD). Therefore, avoid applying static discharges to the front-panel input connectors. Before connecting any coaxial cable to the connectors, momentarily short the center and outer conductors of the cable together. Avoid touching the front-panel input connectors without first touching the frame of the instrument. Be sure the instrument is properly earth-grounded to prevent buildup of static charge.

Connector Savers

Connector savers are useful in prolonging instrument life and ensuring better quality measurements. Refer to the following table for a list of commonly used connector savers.

Connector Savers
Connector Part Number Comments
7 mm   Not available
Type-N 50 ohm   Not available
Type-N 75 ohm 85036-60015 Instrument grade
3.5 mm 85052-60013 Metrology grade
3.5 mm 85059C Instrument grade
2.92 mm 11904 2.4 to 2.92 adapters
2.4 mm 85056-60007 Metrology grade
1.85 mm 85058-60009 Instrument grade
1.0 mm   Not available

Do not twist one connector into the other (like inserting a light bulb). This happens if you turn the device body rather than the connector nut. Major damage to the center conductor can occur if the device body is twisted. Use open-ended wrenches on wrench flats on the outer bodies of the connector to help restrict rotation.

Apply force perpendicular to the wrench handle. This applies torque to the connection through the wrench. Do not hold the wrench so tightly that you push the handle straight down along its length rather than pivoting it, otherwise you apply an unlimited amount of torque.

Coaxial Connector Types

The following table shows commonly used RF coaxial connectors. With the exception of the SMA connector, connector types are identified by the diameter (in millimeters) of the air dielectric region as shown in this picture of a 3.5 mm connector.

Types of Coaxial Connectors
Connector Type Frequency Range Coupling Torque Compatible Connectors Notes
1.0 mm Connector
≤ 110 GHz 0.45 Nm
(4 lb-in)
1.0 mm The smallest connector. This connector requires extra care to prevent expensive repairs and repair downtime when making connections.
1.85 mm Connector
≤ 70 GHz 0.57 Nm
(5 lb-in)
2.4 mm 1.85 mm and 2.4 mm connectors are intermateable.
To aid identification, 1.85 mm Keysight connectors have a groove in the male nut and female shoulder. The outer thread size of 1.85 mm and 2.4 connectors is larger than the tread size on SMA, 2.92 mm, and 3.5 mm connectors. This makes the area of the outer conductor's mating surface appear very large compared to the relatively smaller air dielectric.
2.4 mm Connector
≤ 50 GHz 0.9 Nm
(8 lb-in)
1.85 mm
2.92 mm Connector
≤ 40 GHz 0.9 Nm
(8 lb-in)
3.5 mm and SMA 2.92 mm, 3.5 mm, and SMA connectors are intermateable.
2.92 mm and 3.5 mm connectors use the same center pin. Inserting the larger SMA (m) center pin into a 2.92 mm or 3.5 mm connector can slightly degrade the connector. It is recommended that you only mate SMA (m) connectors to other connectors that you reserve for this purpose. SMA connectors use a Teflon dielectric.
3.5 mm Connector
≤ 34 GHz 0.9 Nm
(8 lb-in)
2.92 mm and SMA
SMA Connector
≤ 24 GHz 0.9 Nm
(8 lb-in)
2.92 mm and 3.5 mm