Waveform Histogram Window
Use the waveform Histogram Window dialog box to precisely define the window that is used to construct the histogram. Exact values for each of the four histogram window edges can be entered in this dialog box.
The value limits of the X1, Y1, X2, and Y2 fields depend on the vertical and horizontal scale settings.