Viewing the Phase Noise Analysis Acquisition Settings

To view the phase noise analysis acquisition settings:

  1. In the Phase Noise Setup dialog box, select the Acquisition tab.

  2. The Starting Offset Frequency (fo) field shows the value used in the analysis.

  3. The Time Range field shows the value used in the analysis.

These values are determined by the sample rate and memory depth settings.

Next