Timeout
The Timeout trigger mode triggers when a waveform is above the threshold, below the threshold, or not crossed the threshold (meaning either above of below the threshold) for longer that a specified amount of time.
The Timeout trigger mode is the same as the Pulse Width trigger mode when its Trigger Condition is set to > Time on Timeout.
-
Source — Select one of the analog input channels.
-
Level — Enter the threshold level, use the increase, 50%, or decrease buttons, or turn the front panel Trigger Level knob.
-
Trigger Condition — Specifies the type of timeout:
- High Too Long — Triggers when the waveform is above the threshold level for longer than the specified > Time.
- Low Too Long — Triggers when the waveform is below the threshold level for longer than the specified > Time.
- Unchanged Too Long — Triggers when the waveform has not crossed the threshold level for longer than the specified > Time.