<Comments> Element

Use this optional element to write a comment on the User Measurement Setup dialog box. The comment is typically used to describe the purpose of the measurement and is limited in length to 512 characters. To include line breaks, simply press the keyboard's Enter key as you would when typing in a word processor. For example:

  • <Comments>Before starting the measurement:
  • - Use ESD precautions!
  • - Use only approved cables.
  • - Warm up the DUT.
  • </Comments>

Parent Elements

Child Elements

None

Attributes

None

Example

  • <Measurement>
  • …
  • <Comments>Before starting the measurement:
  • - Use ESD precautions!
  • - Use only approved cables.
  • - Warm up the DUT.
  • </Comments>
  • …
  • </Measurement>