<Measurement> Element

This is the root element of user measurement XML files. This element is required. It declares that the XML file defines a user measurement and not a user function. Always place the <Measurement> element directly after the XML declaration line as shown in example below.

Parent Elements

None

Child Elements

All other elements are descendant elements.

Attributes

The attributes for this element should never be changed and should be copied from the example in this topic.

xmlns:xsi
"http://www.w3.org/2001/XMLSchema-instance"
xsi:noNamespaceSchemaLocation
"Functions.xsd"

Example

  • <Measurement>
  •  
  • …
  • </Measurement>