:ABOR

Syntax

:ABORt

Description

Resets the trigger system and puts the trigger sequence into idle state; turns OFF the continuous activation of the trigger system. (No query)

For more information on the trigger system and each state, see Trigger system.

Related objects

:INIT

:INIT:CONT

Equivalent key

No equivalent keys are available on the front panel.