Retrieving the Results of Rdc Measurement

Other topics about Retrieving Measurement Results

Retrieving Measurement Results

To retrieve only the results of Rdc measurement, use the following command:

As described in Retrieving the Measurement Results for Measurement Parameters 1 through 4, you can also use the following three commands to retrieve the Rdc measurement results along with other data such as the measurement results for measurement parameters 1 through 4:

Retrieving Limit Test Results

To determine whether the Rdc measurement results fall within the limit range (defined with the :CALC:COMP:RDC:LIM command), use the following command:

Also, you can use the *TRG or similar command to retrieve the measurement results as well as the measurement status and then obtain the Rdc measurement limit test results from that measurement status.

As shown below, the measurement status is 0 or 1 when the Rdc measurement results fall within the limit range and 2 or 3 when the Rdc measurement results do NOT fall within the limit range.

Value of Measurement Status

0: Normal

1: Measurement failure (overload)

2: Rdc measurement result did not fall within the limit range

3: Measurement failed and DUT did not fall within Rdc limit.

Sample Program

See the Retrieving Results of Rdc Measurement.