Retrieving the Number of DUTs Sorted into Each Bin (Using the Bin Count Function)

You can use the bin count function to count the number of DUTs sorted into each bin. You can count up to 2,147,483,647 (231-1) DUTs. If this limit is exceeded, the counter value remains at the maximum without being updated.

To turn ON or OFF the bin count function, use the following command:

To retrieve the counter value, use the following command:

Also, you can clear the counter value so that you can re-count DUTs from 0 by issuing the following command:

Other topics about Sorting DUTs Based on Measurement Results