You can use up to eight measurement point setup tables (Tables 1 through 8) to define the signal source and averaging factor for each measurement point. Each measurement point setup table can contain up to 201 measurement points.
When you set measurement points, new settings are applied to the active table. To select the active table, use the following command:
When you manually configure the measurement point setup table, you must add each measurement point to the table and define the various conditions that apply to the specific measurement point. On the other hand, when you use an external controller to configure a measurement point setup table, you can use the following command to define all the measurement points in the active table at once:
You can use the following command to set the unit for the signal source level:
To change only the averaging factor after completion of the calibration/compensation, you may execute the :SOUR:LIST command by specifying the parameter so that only the averaging factor will change with the frequency and signal source level identical to the current settings. In this case, calibration and compensation will be turned OFF automatically; you will need to rerun calibration and compensation.
If you need to change only the averaging factor after completion of calibration or compensation, use the following command:
Execution of the :AVER:COUN command does not turn OFF calibration or compensation automatically.
To delete all entries from each table, issue the following command:
To check the number of measurement points defined in the active table, use the following command:
Other topics about Setting Measurement Conditions