[:SENSe]:AVERage:COUNt <numeric>
[:SENSe]:AVERage:COUNt?
This command sets the averaging factor.
The measurement point for single point measurement, specified with the :SOUR:LIST:POIN command, in the active table, specified with the :SOUR:LIST:TABL command, must be set here.
Execution of this command does not turn OFF calibration or compensation automatically. If you need to change only the averaging factor after completion of calibration or compensation, use this command.
To change only the averaging factor after completion of calibration/compenĀsation, you may execute the :SOUR:LIST command by specifying the paramĀeter so that only the averaging factor will change with the frequency and signal source level identical to the current settings. In this case, calibration and compensation will be turned OFF automatically; you will need to rerun calibration and compensation.
|
Parameter |
Value |
|
Description |
Averaging factor |
|
Range |
1 to 100 |
|
Initial value |
1 |
|
Resolution |
1 |
If your specified parameter is beyond the valid range, the instrument ignores the parameter and uses either the maximum or minimum value depending on whether the parameter is greater than the upper limit or smaller than the lower limit.
{numeric}<newline><^END>
Stim Table > Stimulus tab > Average > {numeric}