List Measurement Display

The list measurement display shown in the following figure appears when you press the List Meas key.

Measurement point number

This is the number of the measurement point set in the measurement point setup display.

Measurement frequency

See measurement frequency.

Averaging factor

See averaging factor.

Oscillator level

See oscillator level (power).

Label 1 to label 4

You can select one parameter for each of the four labels. Click on the parameter column and the Parameter softkey is displayed. Select one of the parameter among the given selection.

Vertical scroll bar

You can scroll the table showing the parameters of each measurement point by moving the scroll bar’s thumb vertically while keeping the mouse button left-clicked and then releasing it at the desired location. You can also scroll the table by clicking the scroll arrows at the ends of the scroll bar or by clicking in the areas in the scroll bar above or below the thumb to move the displayed area one frame up or down, respectively.

Table number

Highlights the active table number. The E4982A has eight tables and each table allows a maximum of 201 measurement points to be set. Use the measurement point setup display to set the measurement point conditions (measurement frequency, averaging factor, oscillator level for the measurement point number) for each table.