Other topics about Using Windows
The E4991B storage contains several partitions. The following table explains the different partitions of the E4991B.
|
Drive |
Description |
|
KBxxx (C:) |
The system drive is replaced with the original image when system recovery is executed. Do not change any files and folders in this. |
|
USER (D:) |
User can keep their files, in this drive. This drive is not replaced even when system recovery is executed. |
|
Factory (E:) |
This drive contains license information and back up data for syscal. The drive is not replaced even when system recovery is executed. Do not change any files in this. |
The E4991B has six USB ports for connecting devices: two in the front panel and four on the rear panel. The main advantages of USB are instant connect and disconnect, and faster data transfer speed.
The first time you plug a device into a USB port there is some wait time. Windows reports that it is identifying the hardware, then searching for the correct driver, then installing the driver (if it is found).
Connecting that same device back into that same port later is quick and easy, but if you move the device to a different USB port, you will have to wait through the hardware ID and driver search again.
Some USB memory may not operate on the E4991B. In that case, try the other kind of USB memory. There are some USB memories which do not work on the front panel USB port, but work on the rear panel USB port.
Keysight Technologies shall not be responsible for, nor assume any liability for data loss in your USB memory device after using it with the E4991B.
Plug & Play capabilities provide both a stable and secured operating environment. You may also notice that it greatly reduces the number of required reboots.
Windows supports DHCP and fixed IP addressing. Also, instant connect and disconnect of the LAN cable, as well as a visual indicator of LAN status in system tray area, makes LAN connections more intuitive. In addition, the Hardware Wizard helps users with system hardware configuration.
By default, Windows allows a double-click method of launching icons. To revert to single-clicking, see the Windows help.
Adding a printer should be done as Windows operation. See Connecting Printer.