About DC control voltage delay, DC power delay and point delay

This section describes the point delay for DC control delay, DC power delay, and common settings of E5052B. For more information about RF Power measurement settings, see Confirming Result of RF Power Measurement.

About delay while DC control is selected for sweep parameter

The following section describes how to set up DC control delay and point delay. For better understanding of each delay, "a," "b," "c" and "e" and the measurement point ā€œdā€ used in the description below, refer to Delay While DC Control Selected for Sweep Parameter.

 Delay While DC Control Selected for Sweep Parameter

About Delay While DC Power is Selected for Sweep Parameter

The following section describes how to set up DC power delay and point delay. For better understanding of each delay, "a," "b," "c" and "e" and the measurement point "d" used in the description, refer to Delay While DC power is Selected for Sweep Parameter.

Delay While DC power is Selected for Sweep Parameter

About Delay in Tester Mode

In the tester mode, measurement is made for only one measurement point. The delay for the measurement point can be set by using a point delay setting.

Delay in Tester Mode