In frequency/power measurement mode, four traces will be displayed at the same time. The four traces consist of two traces in frequency measurement (the unit is Hz and Hz/V), a trace in RF power measurement (the unit is dBm) and a trace in power supply DC current measurement (the unit is mA).
You can select the trace layout from three- or four-division mode. In each trace layout, data will be assigned as Trace Layout. In the four-division mode, the upper-left trace is frequency in Hz unit and the lower-right trace is frequency in Hz/V unit. Refer to Setting Frequency Format and Sensitivity Aperture for selecting the unit (data format).
Press Display > Allocate key.
Press the desired softkey to select the trace layout.
Trace Layout