An error message is displayed against a red background in the instrument message/warning area in the lower-left part of the screen. Touching Entry Off key at the front panel or executing the :DISPlay:MESSage:CLEar command clears the error message. Moreover, about a specific error message, when a sweep is started again, the display of an error message may disappear. Errors caused by operation of a front panel key simply appear on the display; with a few exceptions, these are not stored in the error queue.
The log of an error message,a maximum of 100 pieces are recorded, and it can go back and check from the newest error. The following procedures perform the procedure of elimination of an error check and an error log. This operation can be performed only from a front panel. It cannot be operated by the "SCPI" command.
System > Error Log > View Error Log
System > Error Log > Clear Error Log
An error with a positive error number is one uniquely defined for this instrument. On the other hand, an error with a negative error number is basically one defined for common GPIB devices in IEEE488.2
A B C D E F G H I J K L M N O P Q R S T U V W X Y Z
|
No. |
Message |
Description |
|
120 |
AFC Failed |
This error message appears when the Automatic frequency control function could not follow the fluctuation in the measurement condition or automatic frequency control function was set on, however, the power or control voltage is not being applied to the DUT For the corrective actions, refer to the error message “AFC out of loop” and the warning message “DC output on required in AFC”. |
|
330 |
AFC out of loop |
The Automatic frequency control function could not follow the fluctuation in the measurement condition, and did not converge on the target frequency. Possible problems and corrective action are shown below.
|
|
51 |
A21 flash ROM write error |
This error occurs when writing the system calibration data to ROM on the A21 board fails. Contact Keysight Technologies’ Customer Contact given at the end of this guide or the company from which you bought the device. |
|
311 |
A4/A5 local unlocked |
This error occurs when the internal Local signal of the instrument cannot be unlocked. There is the possibility of a device failure. Contact an Keysight Technologies sales office or the company from which you bought the device. |
|
130 |
Auto Setting failed |
This error occurs when Freq Band, Input Attn and IF gain cannot be set to optimum value according to the input signal. |
|
No. |
Message |
Description |
|
-222 |
Data out of range |
A data element (not violating the standard) outside the range defined by this instrument has been received. This error occurs, for example, when an integer-based command for which the parameter can be rounded exceeds the range of -65536 to +65536 or when a real-number-based command for which the parameter can be rounded exceeds the range of -9.9e37 to +9.9e37. |
|
280 |
DC control overload |
The current through the DC CONTROL connector is too large. |
|
270 |
DC power overload |
The current through the DC POWER connector is too large. |
|
373 |
Downconverter Fan Stop |
This error occurs when the fan of the downconverter stops. Contact Keysight Technologies’ Customer Contact given at the end of this guide or the company from which you bought the device. |
|
354 |
Downconverter IF not found |
This error occurs when the down-converted signal does not fall into the expected IF range. The deviation between the set nominal frequency and the actual input signal's frequency may be too large. Execute the carrier search function, and set a correct nominal frequency. |
|
352 |
Downconverter Oven Cold |
This error may occur due to the unlocked PLL because the oven is not heated sufficiently for some time after the downconverter is turned on. Heat the oven for some time with the power on. |
|
374 |
Downconverter P5V power fail |
This error occurs when the 5-V power of the downconverter fails. A device failure is suspected. Contact Keysight Technologies’ Customer Contact given at the end of this guide or the company from which you bought the device. |
|
353 |
Downconverter Ref Input Level Low |
This error occurs when the level of the 10-MHz reference signal to the downconverter is low. |
|
372 |
Downconverter Ref PLL unlocked |
This error occurs when the PLL circuit of the downconverter is unlocked during measurement. This error may occur when the carrier frequency of the measurement sample is unstable. It may occur also due to the same reason as "Downconverter Oven Cold." |
|
375 |
Downconverter test failed |
This error occurs when the self-test of the downconverter fails. A device failure is suspected. Contact Keysight Technologies’ Customer Contact given at the end of this guide or the company from which you bought the device. |
|
371 |
Downconverter local unlocked |
This error occurs when the local of the downconverter cannot be locked. A device failure is suspected. Contact Keysight Technologies’ Customer Contact given at the end of this guide or the company from which you bought the device. |
|
No. |
Message |
Description |
|
-200 |
Execution error |
An error associated with execution has been generated for which this instrument cannot specify the error message. This code shows the occurrence of an error associated with execution, as defined in 11.5.1.1.5, IEEE488.2. |
|
No. |
Message |
Description |
|
72 |
Failed to copy file |
This error occurs when copying a file (MMEM:COPY command) fails. |
|
74 |
Failed to create directory |
This error occurs when creating a directory (MMEM:MDIR command) fails. |
|
73 |
Failed to delete file |
This error occurs when deleting a file (MMEM:DEL command) fails. |
|
91 |
Failed to execute user defined key |
In the user menu function, this error occurs when a disabled softkey is executed. |
|
61 |
Failed to hide trace |
In the user window, this error occurs when the show trace "OFF" command is executed to turn off the remaining trace on the window. At least one trace should be visible at all times. |
|
60 |
Failed to hide window |
This error occurs when the show window "OFF" command is executed to turn off the remaining window on the screen. At least one window should be visible at all times. |
|
70 |
Failed to read file |
This error occurs when a VBA project file (MMEM:LOAD:PROG command) or other type of file cannot be read normally. |
|
90 |
Failed to stop program |
This error occurs when stopping a program fails. |
|
71 |
Failed to write file |
This error occurs when the display image (MMEM:STOR:IMAG command) for the LCD screen, a VBA project file (MMEM:STOR:PROG command) or other type of file cannot be written normally. |
|
-257 |
File name error |
A file name error. This message appears when an error exists in the file name and thus a command is not executed correctly. This error occurs, for example, when you try to copy to an improper file name. |
|
-256 |
File name not found |
The file name specified is not found and thus the command is not executed correctly. This error occurs, for example, when you try to read a file that does not exist in a disk or a disk is not correctly inserted into the drive. |
|
80 |
File transfer failed |
This error occurs when writing data into or reading data from a file (MMEM:DATA command) fails. |
|
131 |
Failed to find Freq Band |
The current measurement disables to adapt to carrier frequency, which is measurement target. |
|
133 |
Failed to find IF Gain |
This error occurs when the input signal level is high at IF gain setting for frequency band 1-3 in PN/PLL mode. Under this condition auto setting is disabled. |
|
No. |
Message |
Description |
|
213 |
IF A/D overflow |
This message appears when the internal IF level is too high and it exceeds the internal A/D converter input range. In the phase noise measurement, check that the DUT’s carrier signal is within the selected frequency band. Also, the message may appear if a DUT that has a large noise level and an unstable output level is measured. When measuring phase noise in such a case, decrease the IF Gain value or increase the sweep start value if possible. In the spectrum monitor measurement, decrease the DUT’s carrier level, or set the reference level or input attenuator value larger than the current setting. In the transient measurement, decrease the DUT’s carrier level, or set the max input level or input attenuator value larger than the current setting. |
|
260 |
IF Level Overload |
The IF level is too high. Set the input attenuator value larger than the current setting. |
|
312 |
IF not found |
The IF signal cannot be found. Please confirm whether the cable between RF1 IN - OUT and RF2 IN - OUT is connected correctly. When the connection of these cables has the trouble, error message "IF not found" occurs. The downconverter user may find this error message when the user changes the cable connection. In the phase noise measurement,this error occurs when no signal is inputted to the RF IN, or the input level to the RF IN is too low. Also, the message may appear if a DUT that has an unstable output level is measured, or if the carrier frequency of a DUT is out of the specified frequency band. Aside from the above reasons, there is the possibility of a device failure. Contact an Keysight Technologies sales office or the company from which you bought the device. |
|
-224 |
Illegal parameter value |
The parameter value is improperly set. |
|
-282 |
Illegal program name |
This error occurs when a nonexistent VBA program name is specified by the PROG:SEL:NAME command. |
|
-213 |
Init ignored |
Because another measurement is in progress, the request for initiating a measurement (“INIT” command) is ignored. |
|
250 |
Insufficient IF Level |
The IF level is too low. Set the input attenuator value smaller than the current setting. |
|
230
|
Insufficient RF Level |
The input level to the RF IN connector is too low. |
|
50 |
Internal test failed |
Internal test failed
|
|
170 |
Invalid equation label |
The invalid character is received in the label data element |
|
171 |
Invalid equation expression |
The formula data element is invalid. |
|
No. |
Message |
Description |
|
101 |
License installation failed |
This error occurs when an invalid license code is input during installation of the E5001 SSA-J license. |
|
77 |
Load VBA program failed |
This error occurs when loading a VBA program file fails. |
|
No. |
Message |
Description |
|
20 |
Marker search failed |
This error occurs when marker search fails. |
|
-109 |
Missing parameter |
The number of parameters is less than that required for the command, or the parameter has not been entered. |
|
No. |
Message |
Description |
|
351 |
No downconverter unit connected |
This error occurs when the downconverter is not turned on or when the USB cable is not connected even though the downconverter is enabled. Disable the downconverter, turn on the downconverter, or connect the USB cable. |
|
111 |
No signal found |
This error message appears when a carrier is outside the selected frequency band or the attenuator is improperly set during execution of the Carrier to function. Set the attenuator to 0 in case you measure a DUT whose output is less than - 15 dBm. |
|
No. |
Message |
Description |
|
100 |
Option not installed |
The command received has been ignored because of the mismatch between the contents of an option for this instrument and the command. This error is not generated by front key operations. |
|
290 |
Oven Cold |
This error occurs when PLL cannot be locked because the oven is not warm enough after start-up the E5052B. The resolution is to wait until the oven becomes warm. |
|
No. |
Message |
Description |
|
-220 |
Parameter error |
This error message is displayed when a parameter-related error other than Error -221 to -229 occurs. |
|
-108 |
Parameter not allowed |
The number of parameters exceeds that required for the command. See the command reference to confirm the required number of parameters. |
|
200 |
Power on test failed |
This error occurs when the power-on test fails, indicating a failure of the instrument. Contact an Keysight Technologies sales office or the company from which you bought the instrument. |
|
40 |
Printer error |
This error occurs when the previous printing is still in progress or the printer fails (offline, short of paper, etc.) at the time of outputting the display image on the LCD screen to the printer (HCOP:IMM command). |
|
41 |
Print failed |
This error occurs when printing fails for reasons other than Error 40, Printer error. |
|
-284 |
Program currently running |
This error occurs when the PROG:SEL:STAT RUN command is executed when the VBA program is in the Run state. |
|
-286 |
Program runtime error |
An error occurring when VBA is executed. |
|
92 |
Program not running |
This error occurs when :PROG:QUER? command is executed when the VBA program is not running. |
|
93 |
Program command error |
This error occurs when :PROG:COMM command is executed and another command is sent for execution before the first command execution is finished. |
|
No. |
Message |
Description |
|
75 |
Recall failed |
This error occurs when reading an instrument status file (State01.sta, etc.) (MMEM:LOAD:STAT command) fails. |
|
291 |
Ref In 1 input not detected |
This error occurs when the external reference input to Ref In 1 port is not detected. |
|
220 |
RF freq out of range |
This error occurs when the DUT’s output frequency is not within the measurement range. |
|
240 |
RF level overload |
This error occurs when the input to the RF IN port exceeds the maximum input level in the measurement. The measurement value obtained in such a case is not correct. In the worst case, a failure (damage to the receiver) may occur. |
|
No. |
Message |
Description |
|
76 |
Save failed |
This error occurs when writing an instrument status file (State01.sta, etc.) (MMEM:STOR:STAT command) fails. |
|
78 |
Save VBA program failed |
This error occurs when saving a VBA program file fails. |
|
210 |
System PLL unlocked |
This error occurs when the PLL circuit of the instrument becomes unlocked while the measurement is in progress. This message may appear if the DUT’s carrier signal is unstable. If this message is displayed in the phase noise measurement, the following problems and corrective actions are shown below.
Verify the spectrum of the DUT’s output signal. Decrease the IF Gain value, or increase the sweep start value when possible.
Stop the frequency modulation.
Insert a low-pass filter between the DUT’s output terminal and the E5052B RF IN connector to eliminate the harmonics component. |
|
211 |
System PLL frequency range over |
This error occurs when the internal PLL circuit becomes unlocked while the measurement is in progress. This error may occur when the frequency of the input signal is out of range. |
|
212 |
System PLL Input overflow |
This error occurs when the internal PLL circuit becomes unlocked while the measurement is in progress. This error may occur when the level of the input signal is too large. |
|
214 |
System FLL unlocked |
This error occurs when FLL version of “210 System PLL unlocked." When the capture range in PN measurement is Normal, it’s 210 and when Wide, 214. |
|
215 |
System FLL frequency range over |
This error occurs when FLL version of "211 System PLL frequency range over." When the capture range in PN measurement is Normal, it’s 211 and when Wide, 215. |
|
-310 |
System error |
One of the errors designated as “system errors” in this instrument has occurred. |
|
No. |
Message |
Description |
|
110 |
Target freq out of range |
This error indicates the 2nd, 3rd, or nth order harmonics is not within the E5052B measurement range. At this time, the previous measurement conditions still remain (any of sweep parameters are not changed). |
|
-223 |
Too much data |
The block-, expression-, or character-string-type program data that have been received conform with the standard but exceed the amount that can be processed under the conditions of the memory or conditions specific to memory-related devices. In this instrument, this error occurs when the number of characters exceeds 254 in a character-string parameter. |
|
-211 |
Trigger ignored
|
This instrument receives and detects a trigger command (“TRIG”) or an external trigger signal, but it is ignored due to the timing conditions (the instrument is not in the wait-for- trigger state, for example). Change the setup so that a trigger command or an external trigger signal can be sent after the instrument has entered the wait-for-trigger state. |
|
320
|
Thermometer out of range |
The internal thermometer reading is out of the proper range. Adjustment or repair is necessary. |
|
132 |
Try wide capture range |
This error occurs when the input level of the input signal is high, and exceeds the input level of the unit. It is recommended to change the Capture range to wide. |
|
No. |
Message |
Description |
|
-113 |
Undefined header |
A command not defined in this instrument, although not illegal in the syntactic structure, has been received. See the command reference and use correct commands. |